Configure a style sheet

Set
Global Style
to edit the styles applied to all graphic objects. Set
Control Styles
to edit the styles applied to specific control objects. Control styles overwrite the global style.
  1. In
    Project view
    , select the style sheet to edit.
    TIP: You can select the default style sheet, add a predefined style sheet, or create your own style sheet. See Add a predefined style sheet or Create a style sheet.
  2. To set the global style that applies to all graphic objects, in
    Properties
    , under
    Global Style
    ,  select
    Edit
    and enter the values.
    TIP: You can create dynamic links instead of entering the values manually. See Create dynamic links.
  3. To create a control style, under
    Control Styles
    , next to
    Object
    styles
    , select
    Add
    .
    For example, create a control style for switch objects.
  4. To rename a control style, hover-over the style name, select
    Edit
    and enter a new name.
  5. To edit a control style, expand
    Object
    styles
    , expand the style name, and then edit the properties by selecting
    Edit
    and entering values.
    TIP: You can also create dynamic links instead of entering the values manually. See Create dynamic links.
  6. To delete a control style, next to the style name, select
    Delete
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal