Apply a global style to the project
Select a style sheet in which to display the
FactoryTalk Optix Application
at runtime.
TIP:
To change style sheets at runtime, see Develop a combo box to pick styles.
Prerequisites
- Configure a global style in a stylesheet. See Configure a style sheet.
- To apply a global style to the project
- InProject view, select eitherNativePresentationEngineorWebPresentationEngine.
- InProperties, inStyle sheet, selectthe style sheet to apply.
The project applies the
Global Style
properties from the selected
style sheet.Provide Feedback