Output Energize (OTE)

The OTE instruction sets or clears the data bit based on rung condition.
Available Languages
Ladder Diagram
Ladder Diagram_Output Energize (OTE)_v1
Operands
IMPORTANT: Unexpected operation may occur if:
  • Output tag operands are overwritten
  • Members of a structure operand are overwritten
  • Except when specified, structure operands are shared by multiple instructions.
Ladder Diagram
Operand
Data Type
Format
Description
Data bit
BOOL
tag
Bit to be modified. There are various operand addressing modes possible for the data bit, see Bit Addressing for examples.
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See Index through arrays for array-indexing faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
The data bit is cleared to false
Rung-condition-in is false
Set Rung-condition-out to Rung-condition-in.
The data bit is cleared to false
Rung-condition-in is true
Set Rung-condition-out to Rung-condition-in.
The data bit is set to true.
Postscan
The data bit is cleared to false.
Example
Ladder Diagram
FTStudio-OTE-LD-EX-V1
When switch is true, the OTE instruction sets Light_01 to true. When switch is false, the OTE instruction clears Light_01 to false.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal