Bit Addressing

Bit addressing is used access a particular bit within a larger container. Larger containers include any integer, structure or BOOL array. For example:
Definition
Example
Description
Variable0
defined as LINT
has 64 bits
variable0.42
This example references the bit 42 of variable0.
variable1
defined as DINT
has 32 bits
variable1.2
This example references the bit 2 of variable1.
variable2
defined as INT
has 16 bits
variable2.15
This example references the bit 15 of variable2.
variable3
defined as SINT
holds 8 bits
variable3.[4]
This example references bit 4 of variable3.
variable4
defined as COUNTER structure
has 5 status bits
variable4.DN
This example references the DN bit of variable4.
MyVariable defined as BOOL[100]
MyIndex defined as SINT
MyVariable[(MyIndex AND NOT 7) / 8].[MyIndex AND 7]
This example references a bit within a BOOL array.
MyArray defined as BOOL[20]
MyArray[3]
This example references the bit 3 of MyArray.
variable5
defined as ULINT
holds 64 bits
variable5.53
This example references the bit 53 of variable5.
Use Bit Addressing anywhere a BOOL typed tag is allowed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal