Library explorer

Use the
Library
explorer to move
FactoryTalk Smart Object
definitions from the
System
explorer for reuse. Reusing
FactoryTalk Smart Object
s improves the modeling for a system or plant. To edit, allocate, and deploy a
FactoryTalk Smart Object
, create an instance of the Smart Object in the
System
explorer. You can also create a FactoryTalk Smart Object definition, Add-On-Instruction, or User-Defined Data Type in the Library explorer.
TIP: In the
Library
explorer, you cannot delete elements that have instances that are used in the project.
To open the
Library
explorer, on the explorer bar, select Library
Library
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal