Explorer bar

The explorer bar appears in the Explorer pane of the open project. Use the icons on the explorer bar to open the various explorers:
Item
Description
 System icon
System
. Open the
System
explorer. Use the
System
explorer to create FactoryTalk Smart Objects and the programs within the System Objects.
Devices icon
Devices
. Open the
Devices
explorer.
Use the
Devices
explorer to view and manage the hardware used in the project.
 Execution icon
Execution
. The
Execution
explorer contains the executable logic of a project. Use the
Execution
explorer to create a controller application and to view and change tasks, programs, and routines.
 Library icon
Library
. Open the
Library
explorer. Use the
Library
explorer to add new definitions of Add-On Instructions and FactoryTalk Smart Objects and to add new Data Types to the project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal