Maybe it’s time to rethink warehouse logistics and material handling.
Research shows that material handling can equal up to 25% of manufacturing labor costs and 15% of overall manufacturing costs. Plus, up to 50% of all workers’ compensation claims are related to manual material handling activities.
As a result, manufacturers are using artificial intelligence (AI) and autonomous mobile robot (AMR) solutions to move materials on their factory floor faster, cheaper and safer.
Since 2015, OTTO® AMR robots and autonomous forklifts have helped companies generate a fast return on investment. This includes decreasing labor by up to 20%, saving more than $1 million annually, and achieving an internal rate of revenue of over 50%.
Billion-dollar consumer goods company chooses AMR robots
Four material handling alternatives were considered

Our autonomous mobile robot fleet can tackle material handling jobs up to 4200 lbs.
A global consumer goods company needed a flexible, reliable and safer solution to improve warehouse logistics across two enormous facilities.
Before the material handling solution was selected, AMR robots, conveyors, forklifts and automated guided vehicles (AGVs) were all evaluated for productivity and costs.
The company discovered OTTO AMR robots were more flexible than conveyors, safer than traditional forklifts, more adaptable than AGVs and the most cost-effective solution. So, AMR robots were selected for both sites. And a positive ROI was delivered in less than two years.
- 1.75 million square-feet total operations across 2 manufacturing facilities
- 1275 AMR robot miles traveled daily
- 6100 missions completed daily
Move materials faster, cheaper, safer with AMR robots
See how to improve your factory and warehouse logistics
CPG
Automotive
Medical
Food & Beverage
Electronics
Industries adopting manufacturing and warehouse robots
AI-powered AMR robots are engineered to work with and around people and factory floors
Need solutions to improve material flow in your manufacturing or logistics facilities? AMR robots help boost personnel productivity, increase safety and deliver fast return on investment. Our 10-year growth has been exponential. And our AMR robot customer base, industries and applications continue to grow. Visit our case studies to see why.
Are AMR robots a good fit for your company? Use our ROI Calculator to get a quick look at your payback period! Some of the top manufacturing industries introducing AMR robots:
- Auto & Tire
- Food & Beverage
- Consumer Products
- Life Sciences
- Warehousing & Logistics
- Printing & Packaging
- Industrial Manufacturing
Top 15 material handling applications for AMR robots
What are the top applications for autonomous mobile robots in your plant? MH Equipment says some of the top material handling and warehouse logistics applications for AMR robots and autonomous forklifts include:
- Replenishment from warehouse staging area to lineside
- Moving from subassembly to main production lines
- Work-in-progress transporting
- Palletizer to stretch wrapper to outbound staging
- Kitting area to lineside
- Final assembly to lineside
- End-of-line to automated storage and retrieval systems (ASRS) infeed
- Delivering goods from storage zones to work cells
- Staging containers between work stages as work-in-progress
- Picking goods and relocating to pack-out stations
- Transporting raw and finished goods among storage locations
- Moving products to pack lines
- Returning over-draws to inventory
- Unloading or stacking boxes
- Offloading pallets and materials from trucks
Smarter. Faster. Easy to program.
Improve Speed and Flexibility
Easily manage your AMR robot fleet and maximize throughput. Scale with intuitive software that pairs job requests and robots in real time, lowering cycle time.
- Select the right AMR robots for the task
- Easily design routes and program function
- Start operating robots in one day
Centralize Fleet Management
Control your entire system from one spot. Integrate your OTTO AMR fleet with your existing systems to seamlessly transfer materials throughout your facility.
- Easily connect with your existing software
- Communicate with your PLCs
- Conveniently issue commands
Easily Scale and Optimize
Analyze and adjust your material handling operations in one place. Maximize your ROI with dashboards that translate data points into action.
- Access live production data
- Troubleshoot any production issues faster
- Identify and maximize trend data
Automating your material handling workflow is easy with our software
Getting started is easier than you think. Start moving materials in one day.


Our software gives you complete control of your material handling operations through one easy-to-use platform. Whether you have one AMR robot or 100 robots, OTTO Fleet Manager software helps get the right products to the right place at the right time, every time. Plus, our AMR robot experts are with you every step of the way – helping you design material handling at peak efficiency.
There’s an OTTO AMR robot for every job
We can improve complex manufacturing and material handling efficiency
OTTO autonomous mobile robots deliver new standards of productivity in your operations with highly reliable material handling solutions that are tailored to your facility’s unique workflows. The result? Customers agree our autonomous robots quickly help improve factory floor throughput, labor efficiency and safety. Which AMR robot is right for you?
- OTTO 100
- OTTO 600
- OTTO 1200
- OTTO 1500
- OTTO Lifter
A strong and agile AMR robot, the OTTO 100 is designed to help move frequent payloads through person-to-person workflows.
Payload capacity: 150 kg (330 lbs.)
Maximum travel speed: 2 m/s (6.5 ft/s)
Total footprint: 740 x 550 x 308 mm (29 x 22 x 12 in)

A tough and nimble AMR robot, the OTTO 600 is engineered to help move mid-sized payloads quickly throughout tight spaces.
Payload capacity: 600 kg (1323 lbs.)
Maximum travel speed: 1.4 m/s (4.5 ft/s)
Total footprint: 1050 x 700 x 320 mm (41 x 27.5 x 12.5 in)

A heavy-duty AMR robot, the OTTO 1200 is designed to help move heavy payloads quickly through tight spaces.
Payload capacity: 1200 kg (2645 lbs.)
Maximum travel speed: 1.5 m/s (5 ft/s)
Total footprint: 1350 x 910 x 320 mm (53 x 36 x 12.5 in)

A heavy-duty AMR robot, the OTTO 1500 is engineered to help you move your heaviest payloads quickly across tough industrial workplaces.
Payload capacity: 1900 kg (4190 lbs.)
Maximum travel speed: 2 m/s (6.5 ft/s)
Total footprint: 1837 x 1283 x 351 mm (72 x 50.5 x 14 in)

A strong autonomous forklift, the OTTO Lifter AMR is designed to help continuously move pallets between stands, machines and factory floor locations.
Payload capacity: 1200 kg (2645 lbs.)
Maximum travel speed: 1.5 m/s (5 ft/s)
Total footprint: 2841 x 1201 x 2155 mm (112 x 47 x 85 in)

Others also viewed
Based on your activity