Target Position Entry - Position

This dialog box provides an easy format for editing Position for MCLM and MCCM instructions. The dialog box title indicates the Coordinate System and Tag Names for the instruction.
Parameters
Target Position Entry Dialog Box Fields
Feature
Description
Axis Name
This column has the names of each axis in the coordinate system named in the ladder faceplate. These names are not editable.
Target Position/Target Increment
The values in this column are numeric. They show the endpoint or incremental departure of the move depending on the active Move Type.
When the Move Type is Absolute, the target column is entitled Target Position and when the Move Type is Incremental, the target column is entitled Target Increment
Actual Position
This column contains the current actual position of the axes in the coordinate system. These values update dynamically when online and the Coordinate System Auto Tag Update is enabled.
Via Position/Via Increment/Center Position/Center Increment/Radius/Center Incremental
Depending on the Circle Type selected, this column contains the Via point position or increment, the Center Position or increment, or the Radius.
This column appears only for MCCM instructions.
Set Targets = Actuals
When in Absolute mode, this button automatically copies the actual position values to the Target Position Column. This button is not active in Incremental mode.
Set Vias = Actuals (MCCM instruction)
This button copies the values from the Actual Position fields to the Vias Fields. It is only active if the instruction type is MCCM, the Move Type is Absolute and the circle type is not Radius or Center Incremental.
OK
Click this button to accept your edits and close the dialog box.
Cancel
Click this button to close the dialog without accepting your edits.
Apply
Click this button to apply your edits and continue editing in this dialog box.
Help
Click this button for help on this tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal