Axis Properties for Ethernet motion system

Use the
Axis Properties
dialog box for an Axis CIP Drive data type to configure integrated motion systems on the EtherNet/IP network. Use the dialog box to:
  • Edit the properties of an axis.
  • View the current state of the axis.
  • View the current state of the CIP Safety drive when the drive is a CIP safety drive.
  • Perform a manual tune function.
The
Axis Properties
dialog box includes these parameters.
Table Heading
Table Heading
Categories
A list of all option categories available for configuration. Select a category and its options appear to the right of the list. When an option changes, a "*" appends to the name of the category. Select
Apply
or
OK
to save the changes.
Axis State
Displays the current state of the axis. These states include:
  • Unconnected
  • Precharge
  • Stopped
  • Starting
  • Running
  • Testing
  • Stopping
  • Aborting
  • Faulted
  • Start Inhibited
  • Shutdown
  • Axis Inhibited
  • Not Grouped
  • No Module
Safety State
Displays the current state of the CIP Safety drive. These states include:
  • Unknown (No Motion Connection)
  • Self-Testing
  • Configured (No Safety Connection)
  • Self-Testing Failed
  • Running
  • Not Running
  • Recoverable Fault
  • Unrecoverable Fault
  • Configuring
  • Not Configured
  • Unknown
  • Not Configured (Torque Permitted)
  • Not Running (Torque Permitted)
    The Safety State is available only when the drive is a CIP safety drive.
Safe Torque Off bypassed
This warning displays when the drive is a CIP Safety drive and Safety State is
Not Configured (Torque Permitted)
or
Not Running (Torque Permitted)
.
The Safe Torque Off safety function may be bypassed when performing a Motion Direct Command while the safety controller is in Program Mode. The CIP Safety drive allows Motion producing power when Safe Torque Off is bypassed.
Manual Tune
Opens the
Manual Tune
dialog box to perform the manual tune function and run the drive.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal