Source Control > Add to Source Control command

Choose this command to initiate a check in operation.
Note that this menu item displays only if all of the following conditions exist:
  • an open project exists
  • no association exists between the open project and any file under source control.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal