Project Documentation Language dialog box overview

Use the
Project Documentation Language
dialog box to turn on the Project Documentation Languages feature by selecting a current language for the project.
Read the message to understand what effect enabling Project Documentation Languages has on the project.
These are the parameters for the Project Documentation Language dialog box:
  • Associate Existing Project Documentation With
    . A list of all possible languages with which to associate existing project documentation.
    Tip:
    There is no specific language selected by default. You can select a language to associate existing documentation with a language.
  • Customs
    . Click to open the Custom Language Configuration dialog box to manage the customized languages in the project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal