Search
Studio 5000 Logix Designer Online Help
Online command failed
The online command (For example, tune or motor/encoder test) to the axis failed. This could occur because:
The attempted command cannot be executed because the axis has not been configured
The attempted command cannot be executed as messaging to the target axis failed
The device does not support the requested operation or service
Studio 5000 Logix Designer
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal