Error - Failed to import component

The component (Program, Phase, or Add-on instruction) could not be imported. This error can occur for the following reasons.
Import target is no longer valid
This error occurs when Online in Remote Run Mode if an Import command cannot be completed because the import target is no longer valid. The specified component is discarded upon import.
Locked component is from a different controller family
A locked component from a different controller family cannot be imported while online. The component must be recompiled to support the current controller and then re-locked.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal