HIM Cradle Status Indicators
TIP:
The status indicators on the HIM cradle do not indicate the status of an installed communication adapter option. If an optional communication adapter is installed, refer to the adapter user manual for the location and description of any status indicators.
HIM Cradle Status Indicators
Color | State | Description |
---|---|---|
Green | Flashing | The product is ready, but not running, with no converter or inverter faults or alarms present. |
Green | Steady | The product is running (that is, the converter and inverter are active) with no faults or alarms present. |
Yellow | Flashing | A start inhibit condition is present in the converter or inverter. The product cannot be started until the start inhibit condition is cleared. |
Yellow | Steady | A type 1 (user configurable) alarm condition is present in the converter or inverter while the drive is not running. The product can be started without clearing the alarm condition. See parameters 10:465 [Alarm Status A] and 10:466 [Alarm Status B]. |
Red | Flashing | A major fault (for example, an EEPROM CRC fault) is present causing converter and inverter modulation to stop. The product cannot be restarted until the fault condition is cleared. See parameter 0:610 [Last Fault Code]. |
Red | Steady | A non-resettable fault (for example, a user FPGA configuration not loaded) is present in the converter or inverter. |
Red /Yellow | Flashing Alternately | A minor fault is present that does not stop converter or inverter modulation. However, the product cannot be restarted until the fault condition is cleared. |
Yellow/Green | Flashing Alternately | The product is running with a type 1 alarm present that does not stop modulation in the converter or inverter. The product can be restarted without clearing the alarm condition. See parameters 10:465 [Alarm Status A] and 10:466 [Alarm Status B]. |
Green/Red | Flashing Alternately | The product is updating the nonvolatile memory for firmware on the main control board, an option card, or a peripheral device. |
Unlit | Off | Main control board is not powered. |
Color | State | Description |
---|---|---|
Unlit | Off | Embedded EtherNet/IP™ is not properly connected to the network or needs an IP address. |
Red | Flashing | An EtherNet/IP connection has timed out. Explicit messaging control timed out. Network address rotary switches have changed or IP address is invalid (defaulting to DHCP) or DHCP lease expired. |
Red | Steady | Adapter failed the duplicate IP address detection test. Rotary switches are set to 888 or the DHCP lease has expired. |
Red/Green | Flashing Alternately | Adapter is performing a self-test. |
Green | Flashing | Adapter is properly connected but is not communicating with any devices on the network. |
Green | Steady | Adapter is properly connected and communicating on the network. |
Color | State | Description |
---|---|---|
Unlit | Off | Adapter is not powered or is not transmitting on the network. |
Green | Flashing | Adapter is properly connected (100 Mbps or 1 Gbps) and transmitting data packets on the network. |
Green | Steady | Adapter is properly connected (100 Mbps or 1 Gbps) but is not transmitting on the network. |
Yellow | Flashing | Adapter is properly connected (10 Mbps) and transmitting data packets on the network. |
Yellow | Steady | Adapter is properly connected (10 Mbps) but is not transmitting on the network. |
Provide Feedback