Reset as Shipped
The
TotalFORCE®
control platform can be reset as shipped using the IP address rotary switches. All parameter data is defaulted. Use the following procedure to perform a reset as shipped.- Power down the product.
- Locate the three IP address switches on the main control board.
- Record the positions of the switches so they can be set back to these positions at the end of the procedure.Hundreds PositionTens PositionOnes Position______________________________________________________
- Set all three switches to position 8, for an overall value of 888.ItemDescriptionAHundreds positionBTens positionCOnes position
- Power up the product. Wait for the STS indicator to turn flashing red and the ENET indicator to turn solid red.
- Power down the product.
- Set the IP address switches to the positions recorded in step 3.
- Power up the product.
Provide Feedback