Recovery Mode

The
TotalFORCE®
control platform has a recovery mode. Recovery mode recreates the product file system and all parameter data is defaulted. Use the following procedure if the processor fails to start up.
  1. Power down the product.
  2. Locate the three IP address switches on the main control board.
  3. Record the positions of the switches so they can be set back to these positions at the end of the procedure.
    Hundreds Position
    Tens Position
    Ones Position
    ______________________________
    ______________________________
    ______________________________
  4. Set all three switches to position 8, for an overall value of 888.
    Drawing of Switches Set to 888
    Item
    Description
    A
    Hundreds position
    B
    Tens  position
    C
    Ones position
  5. Power up the product.
  6. Wait for the STS indicator to turn flashing red and the ENET indicator to turn steady red.
  7. Power down the product.
  8. Set the tens position switch to position 9 and the ones position switch to position 7, for an overall value of 897.
    Drawing of Set Switches to 897
    Item
    Description
    A
    Hundreds position
    B
    Tens  position
    C
    Ones position
  9. Power up the product.
  10. Wait for the STS indicator to turn flashing red and ENET indicator to turn steady red.
  11. Power down the product.
  12. Set the IP address switches to the positions recorded in step 3.
  13. Power up the product.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal