Manually Clear Faults

  1. Press the Clear soft key to acknowledge the fault. CLR icon
    The fault information is removed so that you can use the HIM.
  2. Address the condition that caused the fault.
    You must correct the cause of the fault before you can clear it.
  3. After you complete the corrective action, use one of these methods to clear the fault.
    • Press Stop. If the drive is still running, it stops. Red stop icon
    • Cycle drive power.
    • Select the Clear soft key on the HIM Diagnostic folder Faults menu.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal