History of Changes

This appendix contains the new or updated information for each revision of this publication. These lists include substantive updates only and are not intended to reflect all changes. Translated versions are not always available for each revision.

750-PM101D-EN-P, March 2024

  • New information added to the Apply and Remove Power section.
  • Frame 6L added to the Fan Usage by Product section.
  • Updated the
    PowerFlex®
    755T Lifting/Torque Proving section.
  • Appendix B: Develop Secure Applications added.

750-PM101C-EN-P, June 2023

  • The front cover now indicates that this publication supports Firmware Revisions 10.xxx…12.xxx
  • Firmware Revision 12.xxx did not result in changes to this publication.
    • See publication 750-RD101 for the Firmware Revision 12.xxx parameter list.
    • See publication 750-RD102 for the Firmware Revision 12.xxx conditions list.

750-PM101B-EN-P, April 2022

  • Parameter descriptions and fault, alarm, event, and exception codes are now available in separate publications.
  • Added information on when the Set Defaults operation for a peripheral device also resets the host product.
  • PowerFlex®
    755TS drives added to Fan Usage by Product section
  • Reset as Shipped procedure clarified.
  • Added information on the Recovery Mode function.
  • Added information on the Secure Erase function.
  • Added Appendix A - Permanent Magnet Motors listing.
  • Additional Resources table lists new parameter descriptions and fault, alarm, event, and exception code publications and
    PowerFlex®
    755TS product publications.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal