Signature Authentication
    If a signature for an element cannot be authenticated, the following occurs:
- A warning appears in the Errors pane below the Controller Organizer.
- No signature is shown for the element in the Quick View pane.
For example, if you copy a main routine, but the routine was changed before the copy, warnings appear to indicate that the signature could not be authenticated. No signature appears for the copied routine in the Quick View pane.
Signature Authentication Failed—Warning

Signature Authentication Failed—No Signature

Provide Feedback