Safety Programs
    A safety program has the attributes of a standard program, except that it can be scheduled only in the safety task:
- A safety program can also define program-scoped safety tags.
- A safety program can be scheduled or unscheduled.
- A safety program can contain only safety components.
- All routines in a safety program are safety routines. One safety routine must be designated as the main routine, and another safety routine can be designated as the fault routine.
- A safety program cannot contain standard routines or standard tags.
- For program parameters, a safety parameter cannot be connected with or bound to a standard parameter or controller-scoped tag.
Provide Feedback