Export and Import the Safety Add-On Instruction
    When you export a safety Add-On Instruction, choose the option to include all referenced Add- On Instructions and user-defined data types in the same export file. By including referenced Add-On Instructions, you make it easier to preserve the signatures. When importing Add-On Instructions, consider these guidelines:
- You cannot import a safety Add-On Instruction into a standard controller project.
- You cannot import a safety Add-On Instruction into a safety controller project that has been safety-locked or one that has a safety signature.
- You cannot import a safety Add-On Instruction while online.
- If you import an Add-On Instruction with an instruction signature into a project where referenced Add-On Instructions or user-defined data types are not available, you may need to remove the signature.
For more information, see the Import/Export Project Components Programming Manual, publication 1756-PM019.
Provide Feedback