Device Information View
Use Device Information to view device and status information when the device is
online.
Use Device Information to:
- Determine the identity of the device.
- View the device's current operational state.
- View whether the device was configured by the owner controller.
- View whether an owner controller is currently connected to the device.
- Retrieve the latest information from the device.
- Reset a device to its power-up state.
- If supported, view the Protection Mode of the device.
Device Information View Example

Device Diagnostics
To view the device diagnostics, select Diagnostics in
the Device Information view.
Device Diagnostics Dialog Example

Provide Feedback