Modbus Slave View
Use Modbus Slave view to configure settings for Modbus communication as a Master
slave.
Modbus Slave View Example

Parameter | Definition | Available Choices |
---|---|---|
Modbus Format | Determines whether the Modbus transmission format is Modbus RTU
or Modbus ASCII. |
|
Node Address | Specifies the node address of the slave. | 1…247 (default = 1) |
Diagnostics | When the controller status is online, open the Diagnostics dialog
to view diagnostic counters for performance and error management
with the Modbus Slave. | – |
Select Diagnostics to see the diagnostic information of the Modbus Slave channel.
Modbus Slave Channel Diagnostics Dialog Example

Provide Feedback