Generic ASCII Transmit View
Use Generic ASCII Transmit view to configure parameters for transmitting ASCII data
through serial module.
Generic ASCII Transmit View Example

Parameter | Definition | Available Choices |
---|---|---|
Swap Mode | Determines how the data that is transmitted to the Serial port is
arranged. The swap is performed before the module sends output
data. |
TIP:
A, B, C, and D represent
four adjacent bytes in the received/transmitted data.
|
Termination Mode | Determines the usage of the Termination Delimiters in the
data. |
TIP:
The End Delimiter is only
applied when the tag OxASCII.TxDataLength is set to 0. When
the Ox.ASCII.TxDataLength is greater than 0, the effective
Termination Mode is Ignore End Delimiter.
|
Termination Delimiter 1 | Specifies the channel's first Termination Delimiter. The
Termination Delimiter is used to signal the end of the data.
|
|
Termination Delimiter 2 | Specifies the channel's second Termination Delimiter. |
If you enter $, it means that the Termination Delimiter 2 is not
used. |
Diagnostics | When the controller status is online, open the Diagnostics dialog
to view the diagnostic counters for performance and error
management with the Generic ASCII communication. | – |
Select Diagnostics to see the diagnostic information of the Generic ASCII
Transmit/Receive channel.
Generic ASCII Transmit/Receive Channel Diagnostics

Provide Feedback