Input Eventxx View

The Input Eventxx view, where 'xx' represents the index of an event definition, shows the configuration options available for that event. You cannot configure the parameters from this view, you must use the configuration tags.
Use this view to review the following tasks:
  • Whether the input event is enabled.
  • Whether the input event is latched.
  • Whether independent point triggers for the input event is enabled.
  • Check the trigger condition for the input event.
  • Check the participants and their State Transition behavior for the input event.
Input Eventxx View Example

Event Definition

See Event Output Tag Definitions for the event definition parameters that you can configure using the Event Output tags.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal