Diagnostic Assemblies
- Diagnostic IO-Link Master Assembly A
- Instance ID = 0x801B (32795)
- Size = 232 bytes
Follow the information in the below table to add each member.Diagnostic Assembly Instance 32795NameData TypeSize in BytesRunModeBOOL1InfoBit_Pad1BOOLDiagnosticActiveBOOLCIPSyncValidBOOLCIPSyncTimeoutBOOLInfoBit_Pad5BOOLFieldPowerOffBOOLInfoBit_Pad7BOOLDiagnosticSequenceCountSINT1DiagBit_Pad0BOOL2DiagBit_Pad1BOOLDiagBit_Pad2BOOLDiagBit_Pad3BOOLDiagBit_Pad4BOOLDiagBit_Pad5BOOLDiagBit_Pad6BOOLDiagBit_Pad7BOOLDiagBit_Pad8BOOLDiagBit_Pad9BOOLDiagBit_Pad10BOOLDiagBit_Pad11BOOLFlashUpdateRequiredBOOLSelfTestFaultBOOLDiagBit_Pad14BOOLDiagBit_Pad15BOOLPadDINT4LocalClockOffsetLINT8LocalClockOffsetTimestampLINT8GrandMasterClockIDSINT8ChannelMode00SINT1ChannelMode01SINT1ChannelMode02SINT1ChannelMode03SINT1PadDINT4Ch00Diagnostic_Channel_Struct48Ch01Diagnostic_Channel_Struct48Ch02Diagnostic_Channel_Struct48Ch03Diagnostic_Channel_Struct48 - Diagnostic IO-Link Master Assembly B
- Instance ID = 0x801C (32796)
- Size = 200 bytes
Follow the information in the below table to add each member.Diagnostic Assembly Instance 32796NameData TypeSize in BytesChannelMode04SINT1ChannelMode05SINT1ChannelMode06SINT1ChannelMode07SINT1PadDINT4Ch04Diagnostic_Channel_Struct48Ch05Diagnostic_Channel_Struct48Ch06Diagnostic_Channel_Struct48Ch07Diagnostic_Channel_Struct48 - Diagnostic Counters Base I/O Assembly
- Instance ID: 0x301 (769)
- Size = 16 bytes
Follow the information in the below table to add each member.Diagnostic Assembly Instance 769NameDate TypeSize in BytesRunModeBOOL1Infobit_Pad1BOOLDiagnosticActiveBOOLInfobit_Pad3BOOLInfobit_Pad4BOOLInfobit_Pad5BOOLInfobit_Pad6BOOLInfobit_Pad7BOOLDiagnosticSequenceCountSINT1CIPConnectionsINT2CIPLostPacketsDINT4CIPTimeoutsDINT4CPUUtilizationINT2PadINT2
Provide Feedback