Wiring Related to COM Pins

See the following diagrams for wiring the COM pins on the RTBs when using the 5034-OB8 and 5034-OB8XT modules.
Individual Load Return Wiring on COM Pins
Star-connected Load Return Wiring on COM Pins
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal