SA Power Indicator

Interpret SA Power Indicator – Standard I/O Modules
Indicator State
Description
Recommended Action
Off
The module is not powered or outside its designed operating range.
Complete the following actions:
  1. Confirm that the system is powered.
  2. Confirm that the module is installed properly.
Steady green
There is SA power to the module
None
Steady red
There is no SA power to the module or SA power is not in the valid range.
Complete the following actions:
  1. Confirm that SA power wiring is properly connected to the adapter, expansion power module, or 5034-MBSA mounting base.
  2. Check the following:
    • Check that the SA voltage is in the correct range.
    • If an external power supply is used, confirm that the power supply is turned on.
    • Confirm that there is sufficient voltage supplied to the module.
    • Make sure that the mounting base to mounting base connection is properly secured.
      Go to Chassis Information view in the Module Properties of the adapter module to check the Field Power status of mounting bases installed in all slots.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal