Counters View

Counters is available only if you choose a value for the Counters parameter in the Device Definition dialog.
Counters show the configuration options that are available for each counter. Based on your Input Filter Time selections, the Input Filter Time Off→On and On→Off times change. You can also enable Rollover at Preset. To modify the counter preset value, use
O.Counterxx.Preset
in the controller tags.
Counters View Example
IMPORTANT:
The total number of Counters subtracts from the available number of Points. For example, if you configure a 5034-IB8 module to use four counters, the first four terminals are not available to use as points.
The number of points available on the module in this case is 4. That is, points 4…7.

Ptxx Diagnostics

To view the Ptxx diagnostics, select Diagnostics in the Counters view.
Ptxx Diagnostics Example
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal