Points View
Points is only available if you choose This Controller for the Configured By parameter on
the Module Definition dialog.
You must configure each point to use it in a safety application. The outputs are disabled
by default.
Points View Example

Ptxx Diagnostics
To view the Ptxx diagnostics, select Diagnostics in the Points view.
Ptxx Diagnostics Example

Provide Feedback