Module Info View

Use Module Info to view device and status information when the device is online.
Use Module Info to:
  • Determine the identity of the device.
  • View the device's current operational state.
  • View whether the device was configured by the owner controller.
  • View whether an owner controller is currently connected to the device.
  • Retrieve the latest information from the device.
  • Reset a device to its power-up state.
  • If supported, view the protection mode of the device.
Module Info View Example

Module Diagnostics

To view the device diagnostics, select Diagnostics in the Module Info view.
Module Diagnostics Example
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal