Connection View

Use Connection to define controller-to-device behavior.
IMPORTANT:
For PointMax safety I/O modules, you set the RPI on the Safety view.
  • Select Unicast or Multicast connection to use on the EtherNet/IP network. For more information, see Unicast or Multicast Connection.
  • View the reason for a connection fault.
    TIP:
    If there is a connection fault, the Module Fault area displays the error code with a description that helps you to troubleshoot the module. For more information, see Troubleshoot Your Module.
  • Inhibit the module. For more information, see Module Inhibiting.
    Configure whether a connection failure while the controller is in Run mode causes a major or minor fault.
  • Enable or disable Automatic Diagnostics.
    ATTENTION:
    If you do not enable Automatic Diagnostics, the device does not publish diagnostics to FatoryTalk Alarms and Events.
Connection View Example

Connection over EtherNet/IP

PointMax I/O safety modules support the Connection over EtherNet/IP parameter.
  • With safety input data, you can choose Unicast or Multicast.
  • With safety output data, the connection is set to Unicast and N/A is shown. You cannot change this parameter.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal