Test Outputs Points View
Test Output Points is only available if you choose This Controller for the Configured By
parameter on the Module Definition dialog.
You must configure each point to use it in a safety application. The outputs are disabled
by default.
Test Output Points View Example

Test Output Ptxx Diagnostics
To view the Test Output Ptxx diagnostics, select Diagnostics in the Test Output
Points view.
Test Output Ptxx Diagnostics Example

Provide Feedback