General View

Use General to view the definition of a device, including the device type, revision, electronic keying, connection, and other device-specific values.
General View Example

Module Definition

To change the definition of a device, select Module definition in the General view.
Module Definition Example
Module Definition includes these parameters:
Module Definition Parameters
Parameter
Definition
Available Choices
Series
Specifies the series of the device.
Device-specific
Revision
Specifies the major and minor revisions of the device. The valid range for minor revision is from 1…255.
Device-specific
Electronic Keying
Defines the electronic keying used for the device. Electronic keying compares the device defined in the project to the installed device. If keying fails, a fault occurs.
For detailed information on Electronic keying, see Electronic Keying in Logix 5000 Control Systems Application Technique, publication LOGIX-AT001.
  • Exact Match
  • Compatible Module
Configured By
Determines which tags are generated when configuration is complete.
For the External Means choice, the controller and module establish communication without the controller sending any configuration or output data to the module.
  • External Means
  • This Controller
Input Data
Select the input data type for the device.
  • Safety Data
  • Safety Packed Data

Safety Network Number

The Studio 5000 Logix Designer application automatically assigns a Safety Network Number (SNN) to safety modules as they are added to the project.
The SNN is a time-based number that uniquely identifies subnets across all networks in the safety system. All safety modules in a same system use the same SNN and are automatically assigned the same SNN by default.
The Studio 5000 Logix Designer application assigns an SNN to the first safety module that is added to a remote system. The application assigns the same SNN to additional safety modules that are added to this remote I/O system.
For more information on Safety Network Numbers, see the GuardLogix 5580 and Compact GuardLogix 5380 Controller Systems Safety Reference Manual, publication 1756-RM012.
To change the SNN of a device, select the ellipses next to the SNN field in the General view.
Safety Network Number Example
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal