Unicast or Multicast Connection

During module configuration, you must configure the Connection over EtherNet/IP parameter. The configuration choice dictates how input data is broadcast over the network.
The PointMax I/O modules use one of the following methods to broadcast data:
  • Multicast - Multicast connections deliver information from one sender to multiple receivers simultaneously. Copies of one transmission are passed to a selected subset of possible destinations.
  • Unicast - Unicast connections are point-to-point transmissions between a source node and destination node on the network. A transmission is sent to one destination controller depending on the module configuration.
IMPORTANT: Unicast is the default setting. Use Unicast because it reduces network bandwidth usage. However, if you are using a ControlLogix 5580 controller in a high availability system, you must use Multicast.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal