Device Information View
Use Device Information to view device and status information when the device is online.
You can use this view to complete the following:
- Determine the identity of the device.
- View the device's current operational state.
- View whether the device was configured by the owner controller.
- View whether an owner controller is currently connected to the device.
- Retrieve the latest information from the device.
- Reset a device to its power-up state.
- If supported, view the protection mode of the device.
- Access device diagnostics
Device Information View Example

Provide Feedback