Limits View

Each channel on the analog output module has a Limits view with which it is associated. The Signal Units options correspond to the output type and range for the channel.
You can do the following actions on this view:
  • Disable all the alarms.
  • Latch clamp alarms and configure output claming
  • Enable/disable the output ramping in different modes and configure the ramp rate (if any ramp mode is enabled).
Limits View Example
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal