Calibration Instrumentation Specifications

When you calibrate output modules, use a digital multimeter (DMM) to measure the current or voltage signal the module is sending out. To maintain your module's factory calibration accuracy, use the instrumentation with the specifications listed in the following table.
IMPORTANT: Do not calibrate your module with an instrument that is less accurate than those specified in following table. The following events can result:
  • Calibration appears to occur normally but the module gives inaccurate data during operation.
  • A calibration fault occurs, forcing you to abort calibration. When this happens, I.Chxx.CalFault tag is set for the channel you attempted to calibrate. You can clear this tag by completing a valid calibration or cycling power to the module.
Calibration Instrument Specifications
Catalog Number
Channel Output Type
Calibration Instrumentation Specifications
5034-OF4 and 5034-OF4XT
Current (mA)
DMM with resolution better than 0.15 µA
Voltage (V)
DMM with resolution better than 1.0 µV
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal