Alarms View
Each channel on the input module has an Alarms view. You can do the following actions on
this view:
- Disable all the alarms.
- Enable/Disable latching and set the alarm limits for the process alarms:
- High High
- High
- Low
- Low Low
- Deadband
- Enable/Disable latching and set limit for the rate alarm.TIP: Rate Alarm Limit of 0.0 disables the rate alarm.
Chxx - Alarms View Example

Provide Feedback