Channels View

The Channels view shows an overview of the configuration values for all module channels.
TIP: Not all channel configurations are included in Channels view. To view or change the complete set of the channel configuration and also to view the diagnostics information for the channel, use Chxx view.
You can do the following actions on this view for all the channels:
  • Disable the channel, if desired
  • Change the input type and input range
  • Set the notch filter
  • Enable or disable open wire detection
  • Set the scaling and recalculate all configurations with engineering unit
  • Set digital filter
  • Disable alarms
Channels View Example

Chxx View

The Chxx view, where xx represents the channel number, shows the configuration options available for the respective channel.
You can do the following actions on this view:
  • Disable the channel, if desired
  • Change the input type and input range
  • Set the notch filter
  • Enable or disable open wire detection
  • Set the scaling and recalculate all configurations with engineering unit
  • Set digital filter
  • View channel diagnostics information
TIP: To latch and configure alarm parameters, go to Alarms view.
Chxx View Example

Recalculate Units

Recalculate Units lets you recalculate all configurations with engineering unit after a scaling change. Consider the following:
  • The Recalculate Units option is enabled when the scaling configuration is changed.
  • Upon selecting Recalculate Units option, the recalculated new values based on the new scaling configuration are displayed together with the old values for you to verify before changing.
  • If you select "Yes" to proceed with the change, the new values will be set but it gets applied when you select "Apply/OK".
  • If you select "No" to cancel the change, the old values are retained. You can either select the Recalculate Units again or manually change those configurations based on the new scaling.
Recalculate Units Example

Channelxx Diagnostics

Displays the channel diagnostics information when connected with the module. When online with the module, select the Diagnostics on the Chxx view to see the diagnostic information.
Channelxx Diagnostics Example

Alarms View

Each channel on the input module has an Alarms view. You can do the following actions on this view:
  • Disable all the alarms.
  • Enable/Disable latching and set the alarm limits for the process alarms:
    • High High
    • High
    • Low
    • Low Low
    • Deadband
  • Enable/Disable latching and set limit for the rate alarm.
    TIP: Rate Alarm Limit of 0.0 disables the rate alarm.
Chxx - Alarms View Example
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal