Controller State During Calibration
You must add the module to your Studio 5000 Logix Designer application project, as
described in Add a New Module to a Studio 5000 Logix Designer Application Project,
before you can calibrate it.
The project must be online with the owner-controller to calibrate the PointMax analog
modules. You can calibrate under any of the following conditions:
- The controller is in Program Mode, that is, either Remote Program or Program Mode.Your module must be in Program Mode and not be actively controlling a process when you calibrate it.
- There are no connections to the module.
Provide Feedback