Time Synchronization View
    The Time Sync view is read-only and displays the CIP Sync status
            information about the module when the project is online. The Time Sync category displays
            the following information:
- CIP Sync time synchronization status
- UTC system time
- Grandmaster Clock information
- Grandmaster Clock description
- Local Clock information
Time Synchronization View Example

Grandmaster Clock Description
            The Grandmaster clock description dialog provides
                detailed information about the grandmaster clock. To view the Grandmaster clock
                description, select Description in the Time Sync view.
Grandmaster Clock Description Example

Provide Feedback