Use the Status Indicators for Troubleshooting
    PointMax I/O modules use the following status indicators:
- SA Power Indicator - This indicator operates the same for all PointMax I/O modules.
- Module Status Indicator - This indicator operates the same for all PointMax I/O modules.
- Channel Status Indicator - This indicator operates differently based on the module type you are using.
Provide Feedback