Connections for Safety I/O Modules
    During module configuration, you must define the module. Among the Device Definition
            parameters with safety I/O modules, you must choose how module is configured.
The choice depends on whether the project is downloaded to the controller that owns the
            module configuration, that is, the owner-controller, or to a controller that is
            listening to modules in a project, that is an external means controller.
A real-time data transfer link is established between the controller and the module that
            occupies the slot that the configuration references.
When you download module configuration to a controller, the controller attempts to
            establish connections to each module in the configuration. An owner-controller
            establishes two connections (safety input and safety output). A controller that is
            listening to the module establishes one safety input connection.
Because part of module configuration includes a slot number in the remote I/O system, the
            owner-controller checks for the presence of a module there. If a module is detected, the
            owner-controller sends the configuration. One of the following occurs:
- If the configuration is appropriate to the module detected, a connection is made and operation begins.
- If the configuration is not appropriate to the module detected, the connection request is rejected and the Studio 5000 Logix Designer application indicates that an error occurred.The configuration can be inappropriate for many reasons. For example, a mismatch in electronic keying that helps prevents normal operation.
The owner-controller and external means controller monitors its connection with a module.
            Any break in the connection, for example, the loss of power to a remote I/O system,
            causes a fault. The Studio 5000 Logix Designer application monitors the fault status
            tags to indicate when a fault occurs on a module.
Producer/Consumer Communication
            PointMax I/O modules use the Producer/Consumer communication model to produce data
                without a controller polling them first. The modules produce the data and
                controllers consume it. If the connection is a multicast input connection, then
                mulitple controllers can consume the input data, including the owner-controller and
                external means controller.
Connection Reaction Time Limit With Safety Modules
            Setting the RPI on safety modules is not as straightforward as setting it on standard
                modules. With safety modules, the Connection Reaction Time Limit configuration
                affects the RPI that is used for a module.
The Connection Reaction Time Limit defines the predicted period of safety packets on
                the associated connection. If the Max Network Delay exceeds the Connection Reaction
                Time Limit, a connection fault occurs.
By default, the Connection Reaction Time Limit is four times the RPI.
Use the default values for Timeout Multiplier (2) and Network Delay Multiplier (200).
                The Network Delay Multiplier value is in terms of percentage. Thus, 200 means
                200%.
     IMPORTANT: 
    
To determine what is appropriate, analyze each safety point. The default
                        Timeout Multiplier of 2 and Network Delay Multiplier of 200 creates a
                        worst-case input connection reaction time limit of 4 times the RPI, and an
                        output connection reaction time limit of 3 times the RPI.
Changes to these parameters must be approved only after a thorough review by
                        a safety administrator.
For more information on specifying RPI rates, see the Logix 5000 Controllers Design
                Considerations Reference Manual, publication 1756-RM094.
Provide Feedback