Connection View

Use Connection to define controller-to-device behavior:
  • Set the RPI rate. For more information, see Requested Packet Interval.
  • Select Unicast or Multicast connection to use on the EtherNet/IP network. For more information, see Unicast or Multicast Connection.
  • View the reason of Connection Fault.
    TIP: If there is a connection fault, Connection Fault area displays the error code with description that helps you to troubleshoot the module. For more information, see Troubleshoot Your Module.
  • Inhibit the module. For more information, see Module Inhibiting.
  • Configure fault response for connection failure while the controller is in Run Mode.
  • Enable or disable the Automatic Diagnostics.
    ATTENTION: If you do not enable Automatic Diagnostics, the device does not publish diagnostics to FactoryTalk Alarms and Events.
Connection View Example
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal