Calibration Impacts Data Quality
    When a channel on an analog input module is being calibrated, the Notch Filter setting
            for that channel changes to 10 Hz. The I.Chxx.Uncertain tag is set to 1 for that channel
            until calibration is completed.
Grouped inputs share an Analog-to-Digital converter. As a result when any input channel
            is in the calibration process, the 
I.Chxx.Uncertain
 tag is set to 1 for other
            input channels in that group. This is because the data sampling rate slows for all input
            channels in the group.Provide Feedback