Device Information View
    Use Device Information to view device and status information
        when the device is online.
Use Device Information to:
- Determine the identity of the device.
- View the device's current operational state.
- View whether the device was configured by the owner controller.
- View whether an owner controller is currently connected to the device.
- Retrieve the latest information from the device.
- Reset a device to its power-up state.
- If supported, view the Protection Mode of the device.
Device Information View Example

Device Diagnostics
            To view the device diagnostics, select Diagnostics in the Device
      Information view.
Device Diagnostics Example

Provide Feedback