Calibration View
    The Calibration view provides calibration information for all channels on the module. You can
      do the following actions on this view for all the channels:
- View calibration parameters and calibration status for the currently configured input ranges.
- Perform user calibration for one or multiple channels.
- Revert calibration parameters to the factory default values.
For more information on how to calibrate a module, see Module Calibration (Interactive)
Calibration View Example

Provide Feedback