The Motion Database does not contain data for the following selections:

The Motion Database does not contain data for the following selection(s):
  • Motor Catalog Number
The axis properties dialog will open with these selections set to <none>.
Select
Cancel
in the Axis Properties dialog box to preserve your previous selections. Unless a Motion database with the previous data is available, selecting new data and/or applying these changes may make your project incompatible with your hardware configuration and may be unable to download. See Axis Wizard/Axis Properties - Drive/Motor Tab Overview (AXIS_SERVO_DRIVE).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal