Edit external routine properties

To edit external routine properties:
  1. In the Controller Organizer, right click the active routine and choose
    Properties
    .
  2. In
    Name
    , type a name for the external routine.
  3. (optional) In
    Description
    , enter a description of the routine.
  4. Click the
    Configuration
    tab to configure the rest of the properties of this routine.
  5. Click
    OK
    to close the
    Routine Properties
    dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal